PN7462B v2.2 EMC and Antenna Tuning capacitor value

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PN7462B v2.2 EMC and Antenna Tuning capacitor value

1,734件の閲覧回数
poneponecar
Contributor I

Hi,

I am following the n336911 - AN11706 PN7462 family Antenna design guide (1.1).pdf to fine tune my customized antenna.

As the tutorial showed, it could be divided to two parts: 1. the EMC filter, and 2. the matching circuit.

pastedImage_1.png

When I refer to the schematic of PN7462B v2.2, I found more components than shown in the tutorial, so I tried to match them with the tutorial.

The EMC filter should be C28, C29, C31, C32

Matching should be C35, C37, C47, C49, C40, C41, C43, C46.

Then what's the purpose of C38, C39, C44, C45 as marked in the red circle?

pastedImage_2.png

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,538件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

C45 and C39 are NC parts on that board, and C44 and C38 are part of the EMC Filter, EMC filter capacitances.


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,538件の閲覧回数
poneponecar
Contributor I

Hi Kan,

Thanks for the prompt reply. 

With  C28=120pF, C29=27pF, C31=100pF, C32=27pF, C38=120pF, C44= 120pF, how should I correctly fill these values into the excel sheet?

I assume the C01 is 120+27 = 147pF, and the C02 is 120pF, the computed EMC filter cutoff frequency is 14.2Mhz.

Is it correct?

pastedImage_1.png

Also, is there any particular reason to separate the EMC filter capacitors to two different sides of the PCB?

Thanks,

Jay

0 件の賞賛
返信