Hi ,
Which firmware I need to put on PN7462AU for FCC test? Is there any sample firmware available in SDK ? Please help me in this
Thanks
Aswin
Hello Aswin,
I am sorry, but there is no such thing. Usually real uses cases are utilized for that. You can use PSP Examples, like the BasicDiscoveryLoop Example, or the NXP Cockpit firmware and control the reader from there. With the NFC Cockpit you can easily turn on the RF-Field and issue commands as needed.
Hope that helps,
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------