PN7462AU CCID examples missing from v04_01_01

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN7462AU CCID examples missing from v04_01_01

1,352 Views
rogierhofboer
Contributor I


UM10915 describes to CCID examples

  • phExCcid – this version is supporting contactless and contact interfaces,
  • phExNFCCcid – this version is supporting contactless interface and P2P functionality.

But these are not in the latest downloadable version of SW3683.zip

Please add them again. Thanks!

Labels (1)
0 Kudos
4 Replies

1,029 Views
clayvonmueller
Contributor I

I have access to the docstore, can you point me to the  CCID examples are only in an extended package?

I got feedback that the CCID examples are only in an extended package in the http://docstore.nxp.com/  portal.

Thanks,

Clay

DyOCean

0 Kudos

1,029 Views
13102370205
Contributor I

Do you have CCID example wothout  OS. PN7462AUPspPackageFull-v04_05_00 have a lot of examples.But they donot work.

0 Kudos

1,029 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Rogier,

I got feedback that the CCID examples are only in an extended package in the http://docstore.nxp.com/  portal.

The examples should be available in a later release again.

Regards!

Jorge Gonzalez

0 Kudos

1,029 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Rogier Hofboer:

Thank you for posting this question.

I am checking internally about the availability of such CCID examples. Please give me some time to come back with a response.

Regards!

Jorge Gonzalez

0 Kudos