Hi,
I am trying to communicate with an external SPI slave from the PN7462 firmware.
I use the NXP librairie (PN7462AUPspPackageFull-v04_06_00) and check the resulting signals with an oscilloscope.
Whatever the data I send, the physical output is the same!
Here is the code:
#define PH_SPI_SLAVE_FLASH 0
#define PH_SPIM_MSB_FIRST 1
#define PH_SPIM_BAUD_RATE 0 // 1.0 MHz
#define PH_SPIM_NSSPULSE 0
#define PH_SPIM_NSSPOL 0
#define PH_SPIM_INIT_CRC 0
#define PH_SPIM_APPEND_CRC 0
#define PH_SPIM_CRC_INIT 0
#define PH_SPIM_CRC_OFFSET 0
phStatus_t spi_test()
{
phStatus_t status;
uint8_t buf[4] = { 0xFF, 0x00, 0xFF, 0x00 };phhalSPIM_Configure(PH_SPI_SLAVE_FLASH,
PH_SPIM_MSB_FIRST,
E_SPIM_MODE0,
PH_SPIM_BAUD_RATE,
PH_SPIM_NSSPULSE,
PH_SPIM_NSSPOL);status = phhalSPIM_Transmit(PH_SPI_SLAVE_FLASH,
PH_SPIM_INIT_CRC,
PH_SPIM_APPEND_CRC,
PH_SPIM_CRC_INIT,
4,
buf,
PH_SPIM_CRC_OFFSET);
return status;
}
I also join a screenshot of the resulting waveform (in red SCLK, in blue MOSI).
I have tried many other configurations (parameters, values, etc) without success.
I wonder what I am missing!
Any help would be appreciated!
Thanks in advance!
--
Jean-Pierre
Hello Jean,
i am able to transmit multiple data via MOSI to the slave device using the HAL driver function
but my issue is with Receiving data via MISO .
there is HAL function for it , but my application needs it in interrupt form, that is when i receive data ISR for receive data should be called.
There is this concept of water level interrupt which is bit confusing .Can any one help me to figure out the water level interrupts ? how can it be used for receive SPI data?
or
Are there any other way to receive SPI data via interrupts?
Have you received data in via interrupt ?
REGARDS,
sanath rai
Hi xia s,
I just checked the schematic and it is the SPIM_SSN pin (pin 60).
Regards
The NSS of SPI Master is automatic. It can output the chip selection signal when reading and writing without any other control. Can you provide the phhalSPIM_ChipSelect function?
Regards
Here is the code I have for phhalSPIM_ChipSelect.
I believe it comes from the NXP lib (file phhalSPIM.c v04.09.00).
phStatus_t phhalSPIM_ChipSelect( uint8_t bSlaveSelect, uint8_t bOn)
{
#if PHFL_PARAM_CHECK >= PH_PARAM_CHECK_VERBOSE
/* Check for the maximum allowed baud rate value */
if (bSlaveSelect >= PHHAL_SPIM_MAX_NO_SLAVES)
{
return (PH_ERR_INVALID_PARAMETER| PH_COMP_SPIM);
}
#endif
if(bOn)
{
sSlaveConfiguration[bSlaveSelect].dwConfigReg &= ~(1 << SPIM_CONFIG_REG_NSS_VAL_POS);
}
else
{
sSlaveConfiguration[bSlaveSelect].dwConfigReg |= (1 << SPIM_CONFIG_REG_NSS_VAL_POS);
PH_REG_SET(SPIM_CONFIG_REG, sSlaveConfiguration[bSlaveSelect].dwConfigReg);
}
return PH_ERR_SUCCESS;
}
As far as I can remember, the automatic NSS may make the SPI communication fail since we sometimes need to keep the NSS low all along several transmissions (for example, external flash programming).
Observe the signals with an oscilloscope to better understand what is going on.
Regards
Hi xia s,
Here it is:
3 functions to init the SPI module, write and read data.
PH_NOINIT uint8_t gphDEV_SPI_Hw_Buffer[1024];
uint8_t phDEV_Hw_Spi_Init(void) {
PH_USER_ASSERT(
phhalSPIM_Init(PH_DEV_HW_SPIM_TIMEOUT) == PH_ERR_SUCCESS);
/* SLAVE 0: SPI PERIPHERAL */
PH_USER_ASSERT(
phhalSPIM_Configure(PH_DEV_SPI_SLAVE_PERIPH, PH_DEV_HW_SPIM_MSB_FIRST,
E_SPIM_MODE0, PH_DEV_SPI_CLK_1_0_MHZ,
PH_DEV_HW_SPIM_NSSPULSE, PH_DEV_HW_SPIM_NSSPOL) == PH_ERR_SUCCESS);
return 0;
}
phStatus_t phDEV_SPI_periph_write (uint8_t *data, int16_t data_length)
{
phStatus_t status;
// check length
if(data_length <= sizeof(gphDEV_SPI_Hw_Buffer))
{
// copy cmd to static buffer
memcpy(gphDEV_SPI_Hw_Buffer, data, data_length);
}
else
{
return PH_ERR_LENGTH_ERROR;
}
phhalSPIM_ChipSelect(PH_DEV_SPI_SLAVE_PERIPH, true);
// send command
status = phhalSPIM_Transmit(PH_DEV_SPI_SLAVE_PERIPH,
PH_DEV_HW_SPIM_INIT_CRC,
PH_DEV_HW_SPIM_APPEND_CRC,
PH_DEV_HW_SPIM_CRC_INIT,
data_length,
gphDEV_SPI_Hw_Buffer,
PH_DEV_HW_SPIM_CRC_OFFSET);
phhalSPIM_ChipSelect(PH_DEV_SPI_SLAVE_PERIPH, false);
return status;
}
phStatus_t phDEV_SPI_periph_read (uint8_t *data, int16_t data_length)
{
phStatus_t status;
// check length
if(data_length > sizeof(gphDEV_SPI_Hw_Buffer))
{
return PH_ERR_LENGTH_ERROR;
}
phhalSPIM_ChipSelect(PH_DEV_SPI_SLAVE_PERIPH, true);
// send command
status = phhalSPIM_Receive(PH_DEV_SPI_SLAVE_PERIPH,
PH_DEV_HW_SPIM_INIT_CRC,
PH_DEV_HW_SPIM_CRC_INIT,
data_length,
gphDEV_SPI_Hw_Buffer,
PH_DEV_HW_SPIM_CRC_OFFSET);
phhalSPIM_ChipSelect(PH_DEV_SPI_SLAVE_PERIPH, false);
memcpy(data, gphDEV_SPI_Hw_Buffer, data_length);
return status;
}
Regards
I answer this question myself: do not declare the tx buffer on the stack!
--
Jean-Pierre