Hello Community,
I am working on the PN7462 NFC Controller CCID Example using the MCU Expresso IDE.
So far, I am able to build & run the application in debug mode.
Now, I would like to run the application in release mode. for that, I have made the following configurations.
I am getting the following error...
Error starting process.
Cannot run program "C:\Users\embed\Documents\MCUXpressoIDE_11.2.1_4149\example_ccid\PN7462AU_ex_phExCcid\ReleasePN7462AU\PN7462AU_ex_phExCcid.axf": Launching failed
I am sharing with you screenshots of the software & hardware configurations.
Will you please help me to solve this problem?
Regards,
Shiv Patil.
Hello,
Did you build the project before running it in release mode? Please kindly clarity.
Have a nice day.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------
yes, I have built the code before running it.