PN7462: How to use HSU port to communicate for the CCID example

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN7462: How to use HSU port to communicate for the CCID example

530 Views
shiv_patil
Contributor II

Hello Community,

I am working on the PN7462 NFC development board using the CCID example.

I would like to use the HSU port for communication instead of the USB port.

Will you please help me to know,

1. Is it possible to communicate over the HSU port using the CCID example?
2. Further we want to implement a serial bootloader over the HSU port, will HSU support the serial bootloader?

 

Regards,
Shiv Patil.

0 Kudos
Reply
1 Reply

505 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Did you mean the PN7462 EVK. board? If yes. One can't use HSU port instead of USB Port.

Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

Tags (1)
0 Kudos
Reply