PN7462 EEPROM config file: user_ee.bin version 27.0.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN7462 EEPROM config file: user_ee.bin version 27.0.0

891 Views
gokulkrishna
Contributor I

Where can I download user_ee.bin (27.0.0 version) for flashing pn7462 EEPROM.

#pn7462au#pn7462eeprom‌ 

Tags (2)
0 Kudos
2 Replies

643 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi, gokul

   You don't need to download it.

   if you develope your application with reader libary, you can find it in Reader Lib directery.

   For example:

PN7462AUPspPackageFull-v05_12_00\PN7462AU Software\PN7462AU-FW_v05.12.00_Full\PN7462AU\phHal\phCfg\xml\

  if you are using cockpit to connect board, it will be in the path of installation of cockpit.

For example:

 

PN7462AUPspPackageFull-v05_12_00\PN7462AU Documentation

Have a nice day!

TIC weidong sun

0 Kudos

643 Views
gokulkrishna
Contributor I

Hi, weidong.sun‌ 

   If have the version 28.0.0 of user_ee.bin in my package. I wanted to test the card detection with 27.0.0 version of user_ee.bin. So i wanted to check whether the older version (27.0.0) of user_ee.bin is available online.

0 Kudos