PN7362 Custom Board EEPROM Program using MCUXpresso LPC-LINK2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN7362 Custom Board EEPROM Program using MCUXpresso LPC-LINK2

Jump to solution
1,083 Views
kashyap_gada
Contributor II

Dear Sir,

We have created custom boards using PN7362 RFID Controller. It is understood from the Quick Start Manual, UM10883, Section 6.9 The EEPROM has to be updated first before using any NXP Examples. The flashing of eeprom bin file is failing for me with error attached.

On the same side, Flash Programming works fine. Output Attached.

 

Labels (2)
0 Kudos
1 Solution
1,060 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hello @kashyap_gada ,

 

Is it possible to provide a snapshot to show how you configure the programming? As I know, the base address should be 0x201200 for EEPROM program.

 

Thanks for your patience!

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
2 Replies
1,053 Views
kashyap_gada
Contributor II

Dear Kan,

Thank for your reply.

I was following UM10883, but I didn't double check the EEPROM Address. I corrected the address and then program ran normally.

Thank you for your prompt reply!!!

Regards

0 Kudos
1,061 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hello @kashyap_gada ,

 

Is it possible to provide a snapshot to show how you configure the programming? As I know, the base address should be 0x201200 for EEPROM program.

 

Thanks for your patience!

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos