PN7220 DWL_REQ and A7 Pin

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN7220 DWL_REQ and A7 Pin

287 Views
mcihangir
Contributor II

Hi,

 

Does PN7220 have DWL_REQ pin? How can we enter PN7220 to download mode?

 

The A7 pin (TDA_CS2 interface) will not be used in the application.
The TDA8035 interface is not utilized.
Should I apply a pull-up or pull-down resistor to the A7 pin in this case?

 

Thanks!

0 Kudos
Reply
3 Replies

246 Views
Fabian_R
NXP TechSupport
NXP TechSupport

Hello sir,

This is NXP's customer support. Please take a look at the following Document of the PN7220. In section 8 Firmware update, is mentioned that depending on the use case selected the FW Update will be performed either by the MPU Host or, the Secure MCU.

It should not require to add a resistor to the A7 pin. Please also take a look at the Datasheet pin description, where is mentioned that this pin is mostly used for Contact reader selection using a pull-down resistor.

Best Regards,
Fabian
0 Kudos
Reply

269 Views
vincentthivent
Contributor III

Hi,

What do you mean by download mode?


you can leave the pin  TDA_CS2 free.

Thanks,


Vincent

0 Kudos
Reply

257 Views
mcihangir
Contributor II

Hi Vincent,

The PN7160 IC includes a DWL_REQ pin (D3 on VFBGA64) specifically used to enter firmware download mode. However, I could not find a similar dedicated pin for firmware updates on the PN7220.

Does the PN7220 have a specific pin used for entering firmware download mode, similar to DWL_REQ on the PN7160?

Thanks!

0 Kudos
Reply