PN7160 I2C EVK no NFC tag detected

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN7160 I2C EVK no NFC tag detected

836 Views
jjins
Contributor I

I ran pn7160_nfcDemoApp_poll.
tag is not detected

When I checked with spy, the PCD doesn't seem to respond at all and the RF field doesn't seem to be turned on. What should I do?

Tags (1)
0 Kudos
Reply
5 Replies

764 Views
jjins
Contributor I

Error was resolved with a patch. Please look at the log I posted.

I followed an13287 and it didn't work, so im asking.

0 Kudos
Reply

747 Views
KellyLi
NXP TechSupport
NXP TechSupport

Hello @jjins 

 

Could you share how to generate such log "pn7160_nfcDemoApp_poll.txt"? That is to say, what command did you execute that produced such a file? I'll export the same log and compare it with yours, maybe find where is the problem.

BR

kelly

0 Kudos
Reply

737 Views
jjins
Contributor I

The following values were set in libnfc-nci.conf
APPL_TRACE_LEVEL, PROTOCOL_TRACE_LEVEL

There is also a printf I added in pn7160_nfcDemoApp_poll.txt

0 Kudos
Reply

715 Views
KellyLi
NXP TechSupport
NXP TechSupport

Hello @jjins 

Comparing the logs of running nfcDemoApp_poll, there are two variables in your log that are not enabled, NXP_T4T_NFCEE_ENABLE and MIFARE_READER_ENABLE. Is this causing your device to not work? Please check.

BR

kelly

0 Kudos
Reply

799 Views
KellyLi
NXP TechSupport
NXP TechSupport

Hello @jjins 

 In principle, using the 7160 EVK board based on AN13287 porting should work. And I did a test on Raspberrypi+PN7160 EVK, everything works fine. Therefore, it is recommended that you check your system by referring to chapter 5 of AN13287. Or do you have the same error as below?

KellyLi_0-1701610456400.png

BR

kelly

0 Kudos
Reply