Hi Tom,
There are too many ff during the communication. I think it is software issue, please use libnfc_nci stack from our web with OM5578. The NCI communication should be like below:
Running the NXP-NCI project.
NCI >> 20 00 01 01
NCI << 40 00 03 00 11 01
NCI >> 20 01 00
NCI << 40 01 19 00 03 1e 03 00 08 00 01 02 03 80 81 82 83 02 d0 02 ff 02 00 04 88 10 01 a0
NCI >> 20 02 05 01 00 02 00 01
NCI << 40 02 02 00 00
NCI >> 2f 00 01 01
NCI << 4f 00 01 00
NCI >> 20 03 03 01 a0 14
NCI << 40 03 25 00 01 a0 14 20 57 65 64 20 53 65 70 20 30 34 20 31 30 3a 35 33 3a 31 32 20 32 30 ...
NCI >> 20 00 01 00
NCI << 40 00 03 00 11 00
NCI >> 20 01 00
NCI << 40 01 19 00 03 1e 03 00 08 00 01 02 03 80 81 82 83 02 d0 02 ff 02 00 04 88 10 01 a0
NCI >> 21 00 16 07 04 02 02 05 03 03 01 01 01 02 01 01 03 01 01 04 01 02 80 01 80
NCI << 41 00 01 00
NCI >> 21 01 0c 00 02 01 03 00 01 04 01 03 00 01 05
NCI << 41 01 01 00
NCI >> 20 02 04 01 32 01 60
NCI << 40 02 02 00 00
NCI >> 20 02 1f 02 29 0d 46 66 6d 01 01 11 03 02 00 01 04 01 fa 61 0d 46 66 6d 01 01 11 03 02 00 ...
NCI << 40 02 02 00 00
NCI >> 21 03 15 0a 00 01 02 01 01 01 06 01 03 01 80 01 81 01 82 01 83 01 85 01
NCI << 41 03 01 00
WAITING FOR DEVICE DISCOVERY
Please refer to https://www.nxp.com/webapp/Download?colCode=SW4325&appType=license and https://www.nxp.com/docs/en/application-note/AN11990.pdf for more details.
Hope that helps,
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------