PN7150 with ISO 15693

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PN7150 with ISO 15693

2,250件の閲覧回数
faker_09
Contributor I

I got my OM5578 eval working with an Arduino and Ntag cards. Now I want to add ISO15693 cards but I am somehow stuck. I am using this library: GitHub - ThomasBuhot/arduino-nfc: Near Field Communication (NFC) library for Arduino 

I extended the discover map and discover command:

NCI_MSG_RF_DISCOVER_MAP:
TX: 0x21 0x0 0xD 0x4 0x6 0x1 0x1 0x3 0x1 0x1 0x2 0x1 0x1 0x1 0x1 0x1‍
RX: 0x41 0x0 0x1

NCI_MSG_RF_DISCOVER:
TX: 0x21 0x3 0x7 0x3 0x6 0x1 0x2 0x1 0x0 0x1‍‍‍‍
RX: 0x41 0x3 0x1

but after that I get:

NCI_RX: 0x536872312[3]: 0x60 0x7 0x1
NCI_RX: 0x536872315[1]: 0xA1‍‍
NCI error: unhandled core notification event oid = 7

Any ideas what this response means?

ラベル(2)
タグ(3)
0 件の賞賛
7 返答(返信)

2,036件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

There is issue in the response to the discover map and discover command, the message length is expected to be 4 but you just got 3. Why don't  you use the lib from https://www.nxp.com/webapp/Download?colCode=SW4325&appType=license&location=null ? It also supports Arduino platform.

Have a great day,
Kan

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛

2,036件の閲覧回数
faker_09
Contributor I

Thanks for your reply. It took me some time to port the library to work with Arduino but finally I got it compiling.
Now I get an error when it calls configure core conf NCI. My output is as follows:

NCI >> 20 00 01 01
NCI << 40 00 03 00 11 01 ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff 01 00 00 00 20 22 00 20 00 00 00 00 00 00 00 00 00 00 00 00 ab 73 05 08 20 22 00 20 78 3a 00 20 00 00 00 00 73 75 05 08 20 22 00 20 00 00 00 00 00 00 00 00 00 00 00 00 20 22 00 20 78 3a 00 20 68 57 00 20 ec e5 01 20 d4 e5 01 20 f8 57 00 20 fe f3 10 32 81 76 05 08 00 00 00 00 90 00 00 00 70 57 00 20 17 21 05 08 c8 00 00 00 48 e1 01 20 e8 03 00 00 2d 10 00 00 ff 30 3f 00 c6 00 00 00 01 00 00 00 00 10
NCI >> 20 01 00
NCI << 40 01 19 00 11 01 ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff 01 00 00 00 20 22 00 20 00 00 00 00 00 00 00 00 00 00 00 00 ab 73 05 08 20 22 00 20 78 3a 00 20 00 00 00 00 73 75 05 08 20 22 00 20 00 00 00 00 00 00 00 00 00 00 00 00 20 22 00 20 78 3a 00 20 68 57 00 20 ec e5 01 20 d4 e5 01 20 f8 57 00 20 fe f3 10 32 81 76 05 08 00 00 00 00 90 00 00 00 70 57 00 20 17 21 05 08 c8 00 00 00 48 e1 01 20 e8 03 00 00 2d 10 00 00 ff 30 3f 00 c6 00 00 00 01 00 00 00 00 10
Successfully connected to NXPNCI device
NCI >> 20 02 05 01 00 02 00 01
NCI << 03 1e 03
Error: cannot configure NXPNCI settings

0 件の賞賛

2,036件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Tom,

There  are too many ff during the communication. I think it is software issue, please use libnfc_nci stack from our web with OM5578. The NCI communication should be like below:


Running the NXP-NCI project.
NCI >> 20 00 01 01
NCI << 40 00 03 00 11 01
NCI >> 20 01 00
NCI << 40 01 19 00 03 1e 03 00 08 00 01 02 03 80 81 82 83 02 d0 02 ff 02 00 04 88 10 01 a0
NCI >> 20 02 05 01 00 02 00 01
NCI << 40 02 02 00 00
NCI >> 2f 00 01 01
NCI << 4f 00 01 00
NCI >> 20 03 03 01 a0 14
NCI << 40 03 25 00 01 a0 14 20 57 65 64 20 53 65 70 20 30 34 20 31 30 3a 35 33 3a 31 32 20 32 30 ...
NCI >> 20 00 01 00
NCI << 40 00 03 00 11 00
NCI >> 20 01 00
NCI << 40 01 19 00 03 1e 03 00 08 00 01 02 03 80 81 82 83 02 d0 02 ff 02 00 04 88 10 01 a0
NCI >> 21 00 16 07 04 02 02 05 03 03 01 01 01 02 01 01 03 01 01 04 01 02 80 01 80
NCI << 41 00 01 00
NCI >> 21 01 0c 00 02 01 03 00 01 04 01 03 00 01 05
NCI << 41 01 01 00
NCI >> 20 02 04 01 32 01 60
NCI << 40 02 02 00 00
NCI >> 20 02 1f 02 29 0d 46 66 6d 01 01 11 03 02 00 01 04 01 fa 61 0d 46 66 6d 01 01 11 03 02 00 ...
NCI << 40 02 02 00 00
NCI >> 21 03 15 0a 00 01 02 01 01 01 06 01 03 01 80 01 81 01 82 01 83 01 85 01
NCI << 41 03 01 00

WAITING FOR DEVICE DISCOVERY

Please refer to https://www.nxp.com/webapp/Download?colCode=SW4325&appType=license and https://www.nxp.com/docs/en/application-note/AN11990.pdf  for more details.

Hope that helps,

Have a great day,
Kan

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛

2,036件の閲覧回数
faker_09
Contributor I

I used the software stack from https://www.nxp.com/webapp/Download?colCode=SW4325&appType=license

Seems like the library is not perfectly compatible. We will have to further adjust the library to get it running.

0 件の賞賛

2,036件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

SW4325 contains examples for LPC & Kinetis MCUs, did you port it to another MCU? maybe it is a porting issue.

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛

2,036件の閲覧回数
faker_09
Contributor I

Yes but it is pretty hard to try to get things working when there is no free API documentation available. Very bad to get things done for evaluation.

0 件の賞賛

2,036件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Please refer to linux_libnfc-nci/doc at master · NXPNFCLinux/linux_libnfc-nci · GitHub  for details.

Hope that helps,

Have a great day,
Kan

 


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛