PN7150 read HID iclass DP card

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN7150 read HID iclass DP card

3,313 Views
peterwu
Contributor II

Our pn7150 is work when tap mifare , ntag, felica, 15693 card.

We got some HID iclass DP card.
When I tap it on pn7150 there is no response .

There is also no i2c traffic .

how can we to access HID iclass DP card ?

Tags (2)
3 Replies

2,997 Views
peterwu
Contributor II

I can not find any info about iClass DP card.

I try use NXP TagInfo on android to read iClass DP.  It also no any response.   

I assume iClass DP did not follow standard protocol.

So it can not use on PN7150 .  

0 Kudos

2,997 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

Maybe they are operating at another frequency not supported by the TagInfo App nor the NFC Controller. Please confirm with HID the ISO/IEC of these Tags as a first step.

Best regards,

Ivan.

2,997 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

I am not familiar with those specific Tags. Could you please let us know the ISO/IEC to which they are compliant?

Thank you.

Best regards,

Ivan.

0 Kudos