PN7150 assert firmware crash on second read of ISO-DEP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN7150 assert firmware crash on second read of ISO-DEP

815 Views
alberto1
Contributor I

Following AN11690 we applied NXP modifications to support PN7150 on Android Pie.

Details on chip from logs

getChipType HwVersion : 0x88
getChipType Product : PN548C2
phNxpNciHal_configFeatureList chipType = 3
NxpNci> FW Version: 10.1.a7

Chip is functional and can read NFC cards without issues.

But P2P communication with another Android phone does make the firmware to crash with following log:

09-19 17:21:26.469 D/NxpTml ( 3491): PN54X - I2C Read successful.....
09-19 17:21:26.469 D/NxpNciR ( 3491): len = 4 > 61070101
09-19 17:21:26.469 D/NxpTml ( 3491): PN54X - Posting read message.....
09-19 17:21:26.469 D/NxpHal ( 3491): read successful status = 0x0
09-19 17:21:26.469 I/libnfc_nci( 4350): [INFO:nfc_ncif.cc(423)] NFC received ntf gid:1
09-19 17:21:26.469 I/libnfc_nci( 4350): [INFO:nfa_dm_act.cc(268)] NFC_RF_FIELD_REVT(0x5007)
09-19 17:21:26.470 I/libnfc_nci( 4350): [INFO:NativeNfcManager.cpp(700)] nfaDeviceManagementCallback: enter; event=0x5
09-19 17:21:26.470 I/libnfc_nci( 4350): [INFO:NativeNfcManager.cpp(752)] nfaDeviceManagementCallback: NFA_DM_RF_FIELD_EVT; status=0x0; field status=1
09-19 17:21:26.470 I/libnfc_nci( 4350): [INFO:phNxpExtns_DebugAgc.cpp(88)] EXTNS_DebugAgcCfg ,0:
09-19 17:21:26.470 I/libnfc_nci( 4350): [INFO:phNxpExtns_DebugAgc.cpp(114)] EXTNS_DebugAgcCfg AgcDebug not enabled
09-19 17:21:26.471 D/NxpTml ( 3491): PN54X - Read requested.....
09-19 17:21:26.471 D/NxpTml ( 3491): PN54X - Invoking I2C Read.....
09-19 17:21:26.757 E/WifiVendorHal( 3686): getWifiLinkLayerStats(l.937) failed {.code = ERROR_NOT_AVAILABLE, .description = }
09-19 17:21:26.783 D/NxpTml ( 3491): PN54X - I2C Read successful.....
09-19 17:21:26.783 D/NxpNciR ( 3491): len = 9 > 600006A00003A02000
09-19 17:21:26.783 D/NxpTml ( 3491): PN54X - Posting read message.....
09-19 17:21:26.784 D/NxpHal ( 3491): read successful status = 0x0
09-19 17:21:26.784 E/NxpHal ( 3491): CORE_RESET_NTF received !
09-19 17:21:26.784 E/NxpNciR ( 3491): len = 9 > 600006A00003A02000
09-19 17:21:26.784 E/NxpHal ( 3491): phNxpNciHal_emergency_recovery: abort()
--------- beginning of crash
09-19 17:21:26.784 F/libc ( 3491): Fatal signal 6 (SIGABRT), code -6 (SI_TKILL) in tid 4477 (nfc@1.1-service), pid 3491 (nfc@1.1-service)

This happen just presenting for a second time the phone to the antenna.

Checking the documentation (UM10936) a CORE_RESET_NTF with argument A0 stays for: "An assert has triggered PN7150 reset/reboot" 

Attached the logs of first successful communication.

0 Kudos
1 Reply

603 Views
jimmychan
NXP TechSupport
NXP TechSupport

Which MCU are you using?

0 Kudos