PN7150 and pooling presence check issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PN7150 and pooling presence check issue

1,535 次查看
whowhatwhere
Contributor I

Hi!

We are planning on doing RF testing on the board that incorporates RFID periphery and need to output via console the state of the MIFARE card (present/not present) each second.

I'm writing to the console from the PresenceCheck function that pools the card. See the function below.

The issue is, that after arbitrary amount (sometimes it's 5 seconds, sometimes it's 4 minutes) of time the IC informs microcontroller that the card has been removed even though it's still »connected«. 

I've seen this post: https://community.nxp.com/t5/NFC/Intermittent-presence-check-failures-on-PN7150/m-p/1227999

And I also tried changing the parameter of the CLIF_ANA_RX_REG -> RF_CLIF_CFG_BR_106_I_RXA_P (0xA0, 0x0D, 0x04, 0x34, 0x44, 0x20, 0x00,) from 0x22 to 0x20 which does not seem to do anything substantial. 

So one of my questions is, from this application note: https://www.nxp.com/docs/en/application-note/AN11755.pdf on the page 62 where there is info about CLIF_ANA_RX_REG , I probably should change RX_GAIN parameter to make it more stable, did I even change the correct parameter, or is there anything else that could be the issue here?

Thanks for your time,

Kristjan

 

    case PROT_MIFARE:
    {
    	uint32_t sec = 0;
    	uint32_t min = 0;

    	uint32_t time_now = pdTICKS_TO_MS(xTaskGetTickCount());
    	uint32_t period = 1000;

    	uint32_t scan_time_now = pdTICKS_TO_MS(xTaskGetTickCount());
    	uint32_t scan_period = 500;

    	uint32_t removed_ms = 0;

        do
        {

            //DelayMs(1000);

        	uint32_t time = pdTICKS_TO_MS(xTaskGetTickCount());

            if(time >= time_now + period){

            	uint32_t milliseconds = time;

                sec = milliseconds / 1000;
                milliseconds %= 1000;

                min = sec / 60;
                sec %= 60;

                printf("Card is present. ");
                printf("Timestamp: %02d:%02d:%d \n", min, sec, milliseconds);

                time_now += period;
            }

            // check if card was removed each 100ms
            if(time >= scan_time_now + scan_period){

            	removed_ms = time;

				/* Deactivate target */
				pn7150_writeData(NCIDeactivate, sizeof(NCIDeactivate));
				getMessage(5);
				getMessage(100);

				/* Reactivate target */
				pn7150_writeData(NCISelectMIFARE, sizeof(NCISelectMIFARE));
				getMessage(5);
				getMessage(100);

				scan_time_now += scan_period;
            }

        } while ((rxBuffer[0] == 0x61) && (rxBuffer[1] == 0x05));


        uint32_t seconds  = removed_ms / 1000;
        removed_ms %= 1000;

        uint32_t minutes = seconds / 60;
        seconds %= 60;
        printf("Card removed at: %02d:%02d:%d \n", minutes, seconds, removed_ms);

        break;
    }

 

 

 

0 项奖励
回复
1 回复

1,523 次查看
fangfang
NXP TechSupport
NXP TechSupport

Hello,

For the setting CLIF_ANA_RX_REG. One may refer to the SW4325 as the link.

URL:https://www.nxp.com/products/rfid-nfc/nfc-hf/nfc-readers/high-performance-nfc-controller-with-integr....

Have  a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 项奖励
回复