Hello Everyone,
I have a problem with PN7150 integration with Android Oreo (8.1.0), I've tried to follow the instructions in this doc AN11690.pdf. but still failed. Here I attach some screenshots of the error message.
first, it says I need to add repo init. so I add this command;
repo init -m LINUX/android/.repo/local\_manifest/nxpnfc\_manifest.xml
Downloading Repo source from https://chromium.googlesource.com/external/repo
remote: Counting objects: 265, done
remote: Total 7291 (delta 4910), reused 7291 (delta 4910)
Receiving objects: 100% (7291/7291), 2.65 MiB | 0 bytes/s, done.
Resolving deltas: 100% (4910/4910), done.
fatal: manifest url is required.
can anyone help me with the above problem? thanks in advance.
Best Regards