PN7150 NFC peer to peer Mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN7150 NFC peer to peer Mode

2,178 Views
mesdouaabderraz
Contributor III

Hello,Everybody

I am using two frdm-k64f Each connected to an NFC controller "pn7150",
And I want to make the connection between them in peer to peer active mode, 
I have already tested each of them with the example using the tag card in the "SW3735.rar" library.
Currently I need to know the steps to switch to peer to peer mode.

cordially

Kan_Li

Tags (2)
1 Reply

1,711 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Mesdoua Abderrazek,

It is easy to play the P2P demo, please following the following steps:

1. download demo code into two FRDM-K64Fs via KDS:

pastedImage_2.png

2. put these two FRDM-K64Fs like below:

pastedImage_3.png

3. you may see the echo messages from the HyperTerminal :

pastedImage_4.png

Hope that helps,


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------