Hello,Everybody
I am using two frdm-k64f Each connected to an NFC controller "pn7150",
And I want to make the connection between them in peer to peer active mode,
I have already tested each of them with the example using the tag card in the "SW3735.rar" library.
Currently I need to know the steps to switch to peer to peer mode.
cordially
Hi Mesdoua Abderrazek,
It is easy to play the P2P demo, please following the following steps:
1. download demo code into two FRDM-K64Fs via KDS:
2. put these two FRDM-K64Fs like below:
3. you may see the echo messages from the HyperTerminal :
Hope that helps,
Have a great day,
Kan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------