Dear All:
我使用PN7120做读卡器,卡放在读卡器上,从发送读卡指令到读到数据大概要1s多的时间,请问这是否正常?
使用官方示例程序“NXP-NCI_LPC82X_example”用开发板测试,等待时间也差不多,请问是否可以通过设置参数调整该时间?
谢谢!
Hi,
You may change the TOTAL_DURATION of the discovery period to check if it makes any difference.
The default value is 0x0100, you may change it to lower value.
Hope that helps,
Have a great day,
Kan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Kan,
非常感谢你的回答。
根据上面的方法进行测试,效果不太明显。修改为0x0080和0x0030等待时间减少的都非常少,不太能够感觉出来。