PN5321 saturate card at close proximity

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN5321 saturate card at close proximity

1,068 Views
bernardvisser
Contributor I

We made a custom NFC reader / writer with the PN5321, copying the refrence design from AN10449_1.

We use Mifare Classic 4K cards in our application.

One of our prototypes is giving intermittent problems with card communication. We found that communicatoin with the card stops working if the card is too close to the antenna.

If the card is 6-15mm above the antenna (coil) communication is bad.

If the card is ~30mm away from the antenna communicaiton is reliable.

Any suggestions on what components to alter to reduce the field strength? 

Tags (1)
0 Kudos
Reply
0 Replies