PN532 energy Harvesting with NTAG I2C

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN532 energy Harvesting with NTAG I2C

1,606 Views
kolem_tim
Contributor I

Hello,

Im currently using the Adafruit PN532 NFC-Shield, from which I want to supply an NTAG I2C Antenna with power.

With the Vout of the NTAG I2C I want to power an MCU.

I want to generate an RF-Field to get 3,3V to the Vout Pin of the NTAG I2C to run my MCU.

I do not exactly how to get an RF-Field without sending Messages with the PN532.

I think I have to set the Tx2RFEn and TX1RFEn Bits of the CIU_TxControl Register (0x6304).

When I write an 0x83 into the Register 0x6304 then there is an RF-Field for a few Milliseconds.

If I read the Register 0x6304 after I have set the two Bits, then there is still the value "0x80" in the Register.

Thanks,

timk

0 Kudos
Reply
1 Reply

1,387 Views
IvanRuiz
NXP Employee
NXP Employee

Hi,

Have you verified that Tx2RFEn and Tx1RFEn are not being overwritten in another part of the code before reading CIU_TxControl register?

Regards,

Ivan.

0 Kudos
Reply