PN532 chip specification about the bandwidth and the transmitting power

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN532 chip specification about the bandwidth and the transmitting power

823 Views
minkoocho
Contributor II

Hello,

Anyone knows PN532 chip specification about the bandwidth and the transmitting power?

I could not find the information from the data sheet.

Thanks in advance.

0 Kudos
1 Reply

689 Views
renkebienert
NXP Employee
NXP Employee

Hi Jimmy,

for NFC devices there is no such spec for  bandwidth and the transmitting power.

The "bandwidth" depends on the antenna design is defined in the related NFC / ISO Standards.

Similar for the transmitting power: the related measurements use the NFC / ISO Standards, which define power requirements for the tags (= minimum required field strength), and then define the related operating distances.

However, for comparison the transmitting power can be indirectly derived from driver supply voltage TVDD and the maximum allowed driver current ITVDD.

BR,

Renke

0 Kudos