PN5190B1 can not exit the HDLL mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PN5190B1 can not exit the HDLL mode

993件の閲覧回数
Fanfei
Contributor II

Hello Expert,

I am developing the upgrade function for PN5190B1. Everything was normal during the initial sample verification, but after mass production, about 20% of the upgraded units had abnormal in NFC functions.
After analysis, it was found that after the upgrade of this part of the sample was completed, the HDLL mode was not exited.
After the upgrade is completed, send the DL_RESET command in HDLL mode. If no response from the PN5190 is received, it indicates that the reset was successful.
However, after resetting, when the command to query the version in HDLL mode is sent, it still executes successfully, indicating that the HDLL mode has not been exited.
The CRC_INFO returned by the upgrade integrity check is ffbe000f. By comparing it with the content of Table 7 in the "PN5190 instruction layer", the integrity check has passed.
The firmware version I upgraded to is v2.07. I also tried downloading the v2.09 firmware for an upgrade, but the same issue persisted.
May I ask why the problem of being unable to exit the HDLL mode occurs?

0 件の賞賛
返信
5 返答(返信)

965件の閲覧回数
KaiLi
NXP TechSupport
NXP TechSupport

Hello @Fanfei 

For PN5190B1, the latest FW version is V2.0B, so could you try to update the latest version and to see if the same issue still exists.

0 件の賞賛
返信

961件の閲覧回数
Fanfei
Contributor II

Hello @KaiLi 

Thannks for you reply.

Its still in HDLL mode after update the FW to version V2.0B.

0 件の賞賛
返信

897件の閲覧回数
KaiLi
NXP TechSupport
NXP TechSupport

Hello @Fanfei 

How did you update FW? By NXP's project (SW6592_PN5190 Secure Firmware Downloader Example Code) or NFC Cockpit?

0 件の賞賛
返信

877件の閲覧回数
Fanfei
Contributor II
Hello @KaiLi
I developed the upgrade program based on NXP's demo(SW6592_PN5190 Secure Firmware Downloader Example Code) and the documentation(UM11942_PN5190 instruction layer).
0 件の賞賛
返信

841件の閲覧回数
KaiLi
NXP TechSupport
NXP TechSupport

Hello @Fanfei 

Could you share your code with us?

0 件の賞賛
返信