PN5190 EnBootNormalMode Error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PN5190 EnBootNormalMode Error

3,015 次查看
rayjoel
Contributor I

Hi, supporters!

    We are developing a reader with the PN5190.

    Some readers are failed to initialize the PN5190 when it calls the function phhalHw_Pn5190_EnBootNormalMode, it returns error.

Normally when the PN5190 works well, the initial SPI datas are:

Host Send:4
7F 20 01 00

Host Recv:4
FF 80 00 08

Host Recv:9
FF 01 00 00 00 01 00 00 00

------------------------------------------------

But some PN5190 are always failed to work , the initial SPI datas are:

Host Send:4
7F 20 01 00

Host Recv:4
FF 80 00 0C

Host Recv:13
FF 03 00 00 00 01 00 00 00 03 00 00 00

-----------------------------------------------

How can we fix the problems ?

       

0 项奖励
回复
6 回复数

2,303 次查看
renkebienert
NXP Employee
NXP Employee

Hi all,

sorry for late reply!

We investigated and found some rare issues with fast crystals. These issues can be fixed with these new PN5190 EEPROM settings:

adr. 0x4BD -> 0x94

adr. 0x4BE -> 0x7F

BTW: this applies for every FW.

BR,

Renke

2,062 次查看
dx1
Contributor II

Dear @renkebienert ,

I read the default configuration, the FW is v2.7. It is shown below:

adr. 0x4BD -> 0x7F

adr. 0x4BE -> 0x94

The configuration is just the opposite. Maybe it's written incorrectly, or maybe it's just about to swap the values?

0 项奖励
回复

2,719 次查看
renkebienert
NXP Employee
NXP Employee

Event: FF 80 00 0C 03 00 00 00 01 00 00 00 03 00 00 00

Refer to Instruction layer (nxp.com)

Event Status 0x00 00 00 03:

1) BOOT_EVENT -> OK, to be expected

2) GENERAL_ERROR_EVENT -> not OK, so let us check the 

 

GENERAL_ERROR_STATUS_DATA 0x 00 00 00 03:

CLOCK_ERROR and GPADC_ERROR

This looks like the x-tal does not start properly or fast enough.

For debugging the XTAL_CHECK_DELAY (address 0013h) EEPROM configuration, can be increased:

0xFF instead of 0xF6 (default) increase the interval and releases the start-up time.

However, it might make sense to change the x-tal (design), if it is too slow...

0 项奖励
回复

2,709 次查看
dx1
Contributor II

Hi @renkebienert 

The Firmware versions upgrade to V2.F6 from V2.01,The problem is solved。

But we have a large number of products, Upgrade all is a lot of work, is there a way to fix this problem without upgrading the firmware

0 项奖励
回复

2,716 次查看
dx1
Contributor II

Hi rekebientert,

Thanks for your reply!

We tried the following, but it still doesn't work:

1、XTAL_CHECK_DELAY:0xFF instead of 0xF6

2、Increase reset timing time PHHAL_HW_PN5190_RESET_DELAY_MILLI_SECS:10 ms  instead of 0xF6

The Firmware versions we used is V2.01,could it be because of this?

But we can't update the firmware right now because EnBootNormalMode Error,Is there any way to factory reset?

 

0 项奖励
回复

2,744 次查看
dx1
Contributor II

Hi,I have the same problem, can you solve it?

0 项奖励
回复