Dear community,
is it possible to read out NDEF messages from ISO 14443B Tags with the example software from Expansion Board for the Raspberry Pi?
I´m using a passiv sensor Tag (TI Tida00217) with a RF430CL330HCPW Transponder on it. If it is not possible with the example software how I can use the Type B functionality from the pn 512.
Best regards,
Bassem
Hi Bassem,
I have a script for PN512EV to reader the type B card, you may use it as a reference.
Hope that helps,
Have a great day,
Kan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Kan_Li,
Do you think the API's in 'NFC Reader Library' could be used to read Type 4B tags?
Thanks Kan_Li
that really helps a lot!