PN512 Configuration for NTAG213 and NTAG I2C

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN512 Configuration for NTAG213 and NTAG I2C

2,535 Views
kolem_tim
Contributor I

Hello,

I want to use a PN512 to communicate to an NTAG 213 or an NTAG I2C.

Are there any application notes or examples out there, where an PN512 is configured correctly to communicate with NTAG213 or NTAG I2C.

Or do I have to configure the PN512 by myself?

Tags (2)
0 Kudos
Reply
3 Replies

2,170 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

There is no specific example. Fortunately, it is based on the reading principle of NFC on the reader's side. It would be helpful to refer to the technical data of the Tag of your interest and develop your specific application.

Please refer to the NXP website for more information about the specific Tag in the Documentation section of the product:

NXP Semiconductors | Automotive, Security, IoT 

Regards,

Ivan.

0 Kudos
Reply

2,170 Views
kolem_tim
Contributor I

Hello Ivan,

I want to be able to communicate with a Tag on the NFC Forum Type 2 Standard or ISO 14443A.

Firstly I want to communicate with NTAG213 and when this works, I want to use NTAGI2C.

I just Need to read and write pages of an NFC-Tag.

Im using SPI to communicate with my PN512 module.

At the Moment Im using the PNEV512 blueboard, where I connected MISO, MOSI, SCK and CS to my Microcontroller, so the Antenna should be ok.

My Question is: How can I send Messages over the FIFO buffer?

The datasheet says that you have to write your Bytes into the FIFO-Buffer.

You can do this by writing them into the "FIFODataReg"-Register.

To send Data I Need wo write transmit command in CommandReg.

When I want to read page 0 of an NFC-Tag, in example NTAG213, then I Need to Transfer the following Bytes in the correct order:

0x30(Read-command), 0x00(page of Byte), 0xXX , 0xXX CRC(2 Bytes)

When this sequence of Bytes is sent, the Tag should answer with the Bytes, which are in page 0.

Then I can read "FIFODataReg" to read the received Bytes.

But it does not work.

Could you please help me to send Read and Write Commands with the PN512?

I just Need to know how to configure the configuration Registers and know to send what Bytes in the right order.

Regards,

Tim

0 Kudos
Reply

2,170 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

It would be helpful to refer to the examples available in the NFC Reader Library:

NFC Reader Library|NXP 

Regards,

Ivan.

0 Kudos
Reply