PN512用作为模拟卡

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN512用作为模拟卡

2,879 Views
rolerole
Contributor I

   我这边因为天线比较小,所以想用卡工作模式,同时主动给它供电,想借此达到加强刷卡距离目的。

   但是我看官方的lib库例程,好像没有卡工作模式配置,只有主动被动的IP-1模式,mifare读卡器模式,felica读卡器已经14443读卡器模式,还有一个powerdown模式

想用卡工作模式,有没有相应的教程呢?

Tags (1)
0 Kudos
1 Reply

2,243 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi,

PN512支持卡模拟模式,参看下文:

pastedImage_1.png

你可以去下载NFCReaderLibraryForCLEV663B-04.030.00.011627或更新的版本,里面的readme已经提到这个特性了:

pastedImage_2.png

相关的demo可以参考NfcrdlibEx8_HCE_T4T,需要PNEV512B和LPCXpresso LPC1769 / LPCXpresso 11u68开发板来运行这个demo。


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos