Nt3H2211 reader

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Nt3H2211 reader

1,137件の閲覧回数
rolerole
Contributor I

hello:

   I want to use the ntag (nt3H2211) to develop product,but i have some questions about the reader.

The reader in the Ntag I2C plus explorer ket (OM5569/nt322ER) ,i can not find somewhere to buy.

This ntag is complianted ISO/IEC 14443 part 2 and part 3,  so  if it means it was not compliant ISO/IEC 14443 part 1 and part 4?

I have some other readers ,but it can not to read the data in this ntag,except the first page. the first page  data that i read by other reader is not entirely correctly , the first byte is some others.

Q1: If i don't want to develop the reader, which reader i can choose,and i can buy it easily,

Q2 : If i need to develop the reader ,how i can develop,where i can get the datum about the reader and ntag?

Q3: which is the difference between the readers,if this ntag has a special transfer protocol?

thanks

タグ(2)
0 件の賞賛
1 返信

804件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Role,

    About reader for nt3H2211, see the link: https://community.nxp.com/message/894338?commentID=894338#comment-894338

   

Best Regards,

Weidong

0 件の賞賛