No debug signal output at PN5180-GPO1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

No debug signal output at PN5180-GPO1

968 Views
johannesdev
Contributor III

Hi!

I am using the PN5180 NFC frontent chip with the OM25180FDK and a custumized antenna. I would like to route out several test signals to AUX1, AUX2 and GPO (TX_IRQ) by means of the NFC Cockpit v 2.3. According to the documentation this should be no problem. Although AUX1 and AUX2 works like a charm, I cannot route out a digital signal to GPO.

For example: I set TX_IRQ to AUX1. After a ISO14443a frame was completely transmitted I can find a short pulse using a oscilloscope on AUX1. However, when I route TX_IRQ to GPO1 no pulse can be found.

I can measure a connection between the corresponding pin on the PN5180 and the J302 pinheader.

Any ideas what I am doing wrong?

Best regards,

Johannes

Labels (1)
Tags (2)
0 Kudos
2 Replies

755 Views
christianeisend
NXP Employee
NXP Employee

Hi Johannes,


just a quick guess: Did you enable the output driver for GPO1? --> Register 0x5, bit 0 --> set to 1

Christian.

755 Views
johannesdev
Contributor III

Oh no! You were right, I forgot to enable the output driver. Thank you very much!

LG Johannes

0 Kudos