NXP Tag Writer: write txt file with line feed character inside

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NXP Tag Writer: write txt file with line feed character inside

4,309件の閲覧回数
matteoboaro
Contributor I

Hello

I'm tryng to write a txt file with line feed character (LF: 0xA) inside but the APP doesn't seems to work for my case:

On APP I'm using Write tags->write from CSV->myfile.txt

myfile.txt content example:

Text;VER=01
R1=0054
R2=00B4
R3=00C4

After the selection of my file the APP show only the following content on the screen:

VER=01

Any suggestion?

Thank you very much

Mat

タグ(2)
0 件の賞賛
返信
3 返答(返信)

3,891件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

please read the user's manual for the format of the csv file

https://inspire.nxp.com/tagwriter/tag-writer-user-manual.pdf 

0 件の賞賛
返信

3,890件の閲覧回数
matteoboaro
Contributor I

Dear Jimmy Chan

I have already read the manual.

It’s not a formatting problem, It’s a LINE FEED problem . Can you try to replicate my situation?

Thank you very much

Matteo Boaro

Electronic Design Department

Software R&D

I. Z. Conce 60011 Arcevia (AN) IT

' (+39) 0731 989865

• matteo.boaro@aristonthermo.com<mailto:matteo.boaro@aristonthermo.com>

Da: jimmychan

Inviato: lunedì 6 agosto 2018 17:34

A: Matteo Boaro <Matteo.Boaro@aristonthermo.com>

Oggetto: Re: - Re: NXP Tag Writer: write txt file with line feed character inside

NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: NXP Tag Writer: write txt file with line feed character inside

reply from jimmychan<https://community.nxp.com/people/jimmychan?et=watches.email.thread> in NFC - View the full discussion<https://community.nxp.com/message/1042838?commentID=1042838&et=watches.email.thread#comment-1042838>

0 件の賞賛
返信

3,890件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

I tried and it cannot read the linefeed character from the CSV file. I think the APP cannot recognize the linefeed.

You may feedback this to nfcapp.support@nxp.com.

0 件の賞賛
返信