NXP SL3S1003/1013 NXP’s UCODE G2iM series transponder ICs - has Any body tried it with battery

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP SL3S1003/1013 NXP’s UCODE G2iM series transponder ICs - has Any body tried it with battery

1,144 Views
anil_gupta61
Contributor I

NXP  SL3S1003/1013 NXP’s UCODE G2iM series transponder  ICs - Has any body tried it with battery power & how was its performance with battery power? Any other design help for antenna & pcb design for this ICs@

Tags (1)
0 Kudos
Reply
1 Reply

947 Views
rfidtag
Contributor II

Hi, Yes we have tried .

When we used the external battery the reading distance was better. You have to a little bit modify input impedance of antenna as  chip input impedance  is not the some in passive  and BAP mode. The reading distance in free air in BAP mode 2W/ERP was about 25m all depend on antenna design and impedance matching.

One important note, the input impedance of chip  is variable and depend on power that is comming on input of chip.

0 Kudos
Reply