NXP NFC Library v07.10.00 and Linux 6.6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP NFC Library v07.10.00 and Linux 6.6

1,705 Views
eldar
Contributor I

Hi, 

Are there any plans to upgrade the NFC library to support Linux 6.6.x ? 

In Linux 6.6.x,  using GPIO through the /sys/class/gpio filesystem is no longer supported, thus the NFC library cannot be used.  The NFC library is using that API to control PN5180 Frontend Reset, Busy, IRQ and DWL signals.

 

Labels (2)
0 Kudos
Reply
2 Replies

1,692 Views
kowalski_analysis
Contributor II

Maybe this guide helps:
https://community.nxp.com/t5/NFC-Knowledge-Base/Porting-PN7160-NCI2-stack-to-Raspberry-Pi-5-OS-Bookw...

It explains how to port the NFC library to support the newer kernel version.

1,677 Views
eldar
Contributor I

Thanks, I will look into it!

0 Kudos
Reply