NTAG213 NFC Tab design

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NTAG213 NFC Tab design

3,861 Views
pylin
Contributor I
  1.        If we design NFC antenna according to AN11276.pdf (attached), do we still need matching circuit between coil and NTAG213
  2.         According to attached excel document, we need to input coil capacitance (Printed: 2-4pF) and turn Exponent (Printed 1.7-1.8) to the excel table for antenna parameter calculation. Please tell me how to determinate these two value based on PCB parameter (for example dielectric constant, pcb thickness)
  3.       Please tell me how to determine connection capacitance (0.5 – 2pF) inside the attached excel file
  4.      Please also send me the NTAG213 application circuit (MOA8 package)( any external component required), packet outline and foot print recommendation. I cannot get the information on web
  5.       Because of the size limit, we want to do 2 layer design. Inside the attached excel file if we set Number of layers to 2, what should we input to the Number of turns item(number of turns of single layer or sum of the two layers). Besides, please give me design example (gerber and excel file ) of multiple layer PCB coil design
  6.      Please send above information to email pylin@grpdfond.com
0 Kudos
Reply
1 Reply

3,617 Views
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

Dear Lin Fiske

  1.         If we design NFC antenna according to AN11276.pdf (attached), do we still need matching circuit between coil and NTAG213

                   A. The tag does not have a matching circuit are you talking about the reader?

 

  1.         According to attached excel document, we need to input coil capacitance (Printed: 2-4pF) and turn Exponent (Printed 1.7-1.8) to the excel table for antenna parameter calculation. Please tell me how to determinate these two value based on PCB parameter (for example dielectric constant, pcb thickness)

            A. Please check sections 4.7.1.4 Determination of turn exponent p 

Calculation of the objective antenna inductance Lo,i 

4.7.2.2 

  1.       Please tell me how to determine connection capacitance (0.5 – 2pF) inside the attached excel file
    1. As explained in section 4.2.3 this is an estimation
  2.      Please also send me the NTAG213 application circuit (MOA8 package)( any external component required), packet outline and foot print recommendation. I cannot get the information on web
    1. In the packae of the application note for NTAg you can find some designs of antenna available
  3.       Because of the size limit, we want to do 2 layer design. Inside the attached excel file if we set Number of layers to 2, what should we input to the Number of turns item(number of turns of single layer or sum of the two layers). Besides, please give me design example (gerber and excel file ) of multiple layer PCB coil design
    1. As you can see the section 2.3.4 apply for PCB antennas
0 Kudos
Reply