NTAG NT3H2111 Pass Through Mode doesn't work

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NTAG NT3H2111 Pass Through Mode doesn't work

2,589 Views
matanyaniv
Contributor II

Hi,

I am trying to use the NTAG NT3H2111 2K pass through mode with no success at all. First I programmed and checked the following: read session register, write session register, read memory (16 bytes), write memory (16 bytes).

Following a presentation of pass through mode and the instructions on the datasheet I tried implementing pass through mode as follows:

1) On session register NC_REG (00h): set PTHRU_ON_OFF=1b (#6 bit), set TRANSFER_DIR=0b( From I2C to NFC, #0 bit) - this step can be done on "1 shot"
2) Wrtie 64 byets to the SRAM - 16 bytes at a time for 4 cycles (Loop)
3) Set NS_REG (06h) bit SRAM_RF_READY (#3 bit) to be 1b. I2C_LOCKED (#6 bit) is automatically reset to 0b to set the tag in the arbitration idle state. The RF_LOCKED (#5 bit) bit is then automatically set to 1b
4) Do polling on NS_REG (06h) bit SRAM_RF_READY (#3 bit) - wait for it to be 0b
5) Write to the SRAM again 

I'm not sure if this is the right way to do it. Is there anything else I'm missing?

Thanks,

Matan 

0 Kudos
Reply
7 Replies

2,018 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Matan,

As the data sheet says"The pass-through mode can only be enabled via I2C interface when both interfaces are
powered." so have you checked if the RF field is already available at the beginning of the pass-thru mode?

Please kindly refer to the following for more details.

pastedImage_1.png

Hope that helps,


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,018 Views
matanyaniv
Contributor II

Hi Kan Li,

Thank you for your answer.

What I described in the implementation is I2C -> NFC direction (you referred to NFC ->I2C direction). Anyhow, NS_REG bit RF_FIELD_PRESENT works well and recognize the mobile phone.

Since I don't use FD pin it's irrelevant for the sequence I described. Is my sequence correct?

Will it be easier to use FD pin instead of polling NS_REG?

On the datasheet it says that " Set NS_REG (06h) bit SRAM_RF_READY (#3 bit) to be 1b. I2C_LOCKED (#6 bit) is automatically reset to 0b to set the tag in the arbitration idle state. The RF_LOCKED (#5 bit) bit is then automatically set to 1b"  But I think none of the automatic bit changes  occur.

Can you please advise?

Thanks again,

Matan 

0 Kudos
Reply

2,018 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Matan,

It depends on how you implement your application, if you prefer interrupt driven mode, FD detect is better.


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,018 Views
matanyaniv
Contributor II

Hi Kan Li,

I've done some more debugging on my sequence and I think I know where is the problem: After writing to the SRAM - NS_REG is set to 41h (I2C_LOCKED = 1b and RF_FIELD_PRESENT= 1b)

According to the description on the datasheets, I need to set SR_RF_READY to 1b and then automatically I2C_LOCKED needs to turn to 0b.

 I want to confirm the MASKING and REGDAT stages for this change:

NS_REG prior to the change: 41h, after change: 21h

 option 1: If SR_RF_READY bit sets all the other bits automatically than

                     MASKING: 08h

                     REGDAT: 49h

option 2: if SR_RF_READY bit does not sets all the other bits automatically than

               MASKING: 68h

               REGDAT: 29h

An example for something I have already done and works:

to turn ON pass through mode: I changed NC_REG from 01h to 40h by MASKING: 41h , REGDAT: 40h.

can you please advise?

Update: I tired to force NS_REG to be 29h: meaning RF_LOCKED bit = 1b ,SRAM_RF_READY = 1b, RF_FIELD_PRESENT = 1b (since the mobile phone is connected - on top of the antenna) -> after writing to the SRAM, but NS_REG value did not changed at all

Many thanks,

Matan

0 Kudos
Reply

2,018 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Matan,

I am sorry, but in my understanding, RF_LOCKED bit ,SRAM_RF_READY and RF_FIELD_PRESENT are status bits, force writing may not take effect, and only the tag may change them in some condition. Please refer to the following for details.

pastedImage_1.png


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,018 Views
matanyaniv
Contributor II

Hi Kan Li,

Thank you very much for clarifying.

I would like you to help me understand what triggers the bit change under this sequence:

pastedImage_1.png

is bit SRAM_RF_READY being triggered by finishing WRITE command? or: by finish writing to FBh of the SRAM?

currently I can switch ON pass through mode and conduct the writing, but I want to trigger NS_REG so the mobile App will collect the data.

Thanks,

Matan

0 Kudos
Reply

2,018 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Matan,

I think it should be by finish writing to the terminator block FBh of the SRAM.


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------