Hello sir,
Yes the CLRC663 does support Ntag I2C passthrough. The issue is that the example from the NFC Reader Library is only, reading specific pages of the NTAG I2C. Once the passthrough is enabled in the NTAGI2C, the CLRC663 needs to read directly to sector 0, page address 0xF0. As mentioned in section 11.3.1 the use of Fast Read commands are recommended.
Please keep in mind that both interfaces cannot be accessed at the same time and the status registers need to be implemented in your application using NS_REG.
Also, keep in mind that in order to access SRAM is required to power on the device via VCC
Unfortunately, we don't have a specific implementation for this in the Library examples.
If you could please share your application output and/or implementation. We may be able to provide further help.
Best Regards,
Fabian