NTAG 5 link Energy harvesting enabled. Can the NTAG5 link EEPROM read and write?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NTAG 5 link Energy harvesting enabled. Can the NTAG5 link EEPROM read and write?

747 Views
join_ren
Contributor III

Dear NXP:

 

NTAG 5 link Energy harvesting enabled. Can the NTAG5 link EEPROM read and write?

0 Kudos
2 Replies

735 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello.

>> NTAG 5 link Energy harvesting enabled. Can the NTAG5 link EEPROM read and write?

Yes. Please note: VOUT and VCC need to be connected as soon as energy harvesting is used. Otherwise
there is no EEPROM access possible from NFC perspective and status registers may
contain invalid information.

Please refer to the more information as the application note.

URL:https://www.nxp.com/docs/en/application-note/AN12365.pdf.

Hope it help you. Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 Kudos

728 Views
join_ren
Contributor III

Hi Fangfang:

 

Got it. Thanks for your support.

0 Kudos