NTAG 5: is possible to set the Passwords also for the RF via I2C bus ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NTAG 5: is possible to set the Passwords also for the RF via I2C bus ?

1,083 Views
cant
Contributor II

Dear Support,

regarding the passwords settings of the NTAG5 family, is possible to set them also for the RFID/NFC communication using the I2C bus ?

I have read this in your AN12366:

7.3 Device Security configuration
The level of security can be defined with the device security configuration
(DEV_SEC_CONFIG) and can be written by both interfaces. If locked by security lock
cannot be updated anymore by any of the interfaces. The IC RF security features can
be chosen between AES tag/mutual authentication or plain password for NTAG 5 boost
(NTA5332) and NTAG 5 link (NTP5332) only. NTAG 5 switch (NTP5210) and NTAG 5
link (NTP5312) only offer plain password.
Form RF perspective there are three levels of security:
• 32-bit plain password
• 64-bit plain password
• AES: Available on NTAG 5 boost (NTA5332) and NTAG 5 link (NTP5332)
Security modes can be configured in DEV_SEC_CONFIG (3Fh).
For I2C perspective only plain password protection is implemented.

So if we wish to set only plain pws for RF and I2C communications, is possible to set the PWs fr the RF communication using the I2C but with the MCU ?

I think yes from this 7.3 paragraph of your AN in this sentence:

The level of security can be defined with the device security configuration
(DEV_SEC_CONFIG) and can be written by both interfaces. 

but I need your confirmation.

Thanks a lot

Labels (1)
Tags (2)
0 Kudos
3 Replies

288 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Dear @amal ,

 

    Could you please create a new post on community or new case via NXP web(support) for the question?

NFC team members will give you feedback as soon as possible.

 

Thanks!

Regards,

weidong

0 Kudos

989 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi Antonio,

   See the descriptions in NTP53x2.pdf, please!

pastedImage_3.png

pastedImage_4.png

pastedImage_5.png

Hope above information is helpful for you!

Have a nice day!

B.R,

Weidong

0 Kudos

309 Views
amal
Contributor I

@weidong_sun Do any of the NTAG5 chip types support SUN type counter based cmac signed memory mapped signatures on NFC read? The NTAG424 supports this as well as mutual authentication, however I am hoping there is an ntag5 that suports protecting the i2c data bus with mutual auth, but also allows a simple cmac signed NFC read we can auth with just a browser no special app.

0 Kudos