NTAG 413 DNA Encrypted communication?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NTAG 413 DNA Encrypted communication?

1,335 Views
yangyouyong
Contributor II

Hi Jonathan , 

Do you have tried the Encrypted write for NTAG413DNA?

As described in doc an410314,  section 5.2.1 Table14, step11.

What is the last 24 bytes mean?

And where are they from?

From the step before. we just can get the Encrypted data and the 16 bytes New IV

So , I was wondering where are the last 24 bytes from ? 

.jonathaniglesias 

0 Kudos
Reply
3 Replies

1,121 Views
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

Dear yang youyong,

I am going to guide you here through the data sheet since this information is under NDA I cannot tell you the information but guide you, as you can see the cmd here is the cmd.WriteData this command, please chekc how this command is constructed,  after the length you can see that there is the data, and the data is the information calculated in step 9, my apologies if I cannot be specific but this information cannot be shared through this communication channel.

BR

Jonathan

0 Kudos
Reply

1,121 Views
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

Dear yang youyong,

I am going to answer this in the internal case  you submitted,since most of this information is under NDA we can guide you through the DS and application notes that are secured so this procedure is clear.

BR

Jonathan 

0 Kudos
Reply

1,121 Views
yangyouyong
Contributor II

Ok, thank you for reminding

0 Kudos
Reply