Hi,
I use NTP53x2 Link in PLM mode and everything works just fine except range.
To improve the range I'm looking at NTA5332 and ALM mode, but as per dev board schematics from here I will have to add a dozen of extra components to connect LAtx and LBtx to the antenna, which seems too complicated for me. Antenna design guidelines document from here is also more like for custom made antennas as I understand, whereas I use the external one from the vendor.
I use this antenna and just a single capacitor for matching.
Am I right with the assumption? Are there easier options to switch from Link to Boost?
Ideally I want to switch to Boost with minimal changes on PCB.
Thanks