NT3H2111WOFHK的焊盘设计

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NT3H2111WOFHK的焊盘设计

906 Views
Guestsun
Contributor II

    1、中间的小焊盘有说明是“metal area not for soldering,是说明中间的小焊端不焊接吗?且此焊盘尺寸未提供。

            请确认下能否中间焊盘焊接,尺寸按0.3*0.3mm设计;

       2、1脚没有给出焊端宽度,1脚和2脚的pin中心距没有给出。

            焊盘设计能否按1脚宽度是0.35mm1脚和2脚的pin中心距为0.55mm设计;

0 Kudos
Reply
2 Replies

892 Views
Tomas_Parizek
NXP Employee
NXP Employee

Hello Guestsun, 

1. Yes, the pad inside is not soldered with the PCB. There is even no soldering pad on the PCB, see below: 

Tomas_Parizek_1-1704889148583.png

 

2. See the dimensions below: 

Tomas_Parizek_0-1704888901390.png

BR

Tomas 

0 Kudos
Reply

904 Views
Guestsun
Contributor II

微信图片_20240109132841.png

0 Kudos
Reply