I have been using the NHS3152 dev boards to prototype for a project and while I am able to flash and run my code while it is connected to my laptop (and transmit data over NFC onto my android phone), it stops working as soon as I disconnect from the laptop.
This behaviour is observed with my own code running on the board and the demo applications supplied. I have already disabled semi hosting. The Blinky application runs (as in debugger shows it is running) but the LED doesn't light up.
Basically, as soon as I disconnect the board, it is no longer recognised by my phone (even though the phone recognises other passive tags). I also connected a source meter to monitor the voltage between Vdd and GND and it falls to 0 even with the NFC field present.
Is the board beyond rescue or can some sort of reset help?