NHS3152 Model의 NFC Chip time resolution (정보처리)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NHS3152 Model의 NFC Chip time resolution (정보처리)

517 Views
obk91
Contributor I

안녕하세요.

NFC Chip (model :NHS3152) 의 spec을 여쭙기 위해 글을 남깁니다.

다름이 아니라, 다른 spec 에 대한 정보는 있지만 정보처리 time-resolution (몇초의 time interval 까지 송수신처리할 수 있는지에 대한 정보) 의 정보가 나와 있지 않아 해당 spec 에 대한 정보를 얻기 위해 질문글을 올립니다.

감사합니다.

0 Kudos
2 Replies

434 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Yes, Please find the NHS3152  document as the link.

 NHS3152: NTAG SmartSensor with Temperature Sensor, Digital and Analog IOs | NXP 

Hope it help you. Have a nice day.

0 Kudos

434 Views
driesmoors
NXP Employee
NXP Employee

Hi,

나는 온라인 번역기를 사용하여 질문을 번역했다. 바라건대 나는 당신의 질문을 올바르게 이해합니다.

The NHS3152 IC is NFC-forum certified and has built-in an NFC controller which is fully compatible with a MIFARE UltraLight Ev1. Using firmware based on the SDK, you can read and write fully NDEF compliant messages, or you can issue low-level APDU commands.

It also has an RTC HW block to keep track of absolute time. It also allows to wake-up the IC from its lowest power mode (Deep Power Down mode) after a configurable time. This interval time has a resolution of seconds, and can be set from 1 second up to ~194 days.

This information can also be found in the datasheet https://www.nxp.com/docs/en/data-sheet/NHS3152.pdf and the hardware user manual https://www.nxp.com/docs/en/user-guide/UM10876.pdf.

Kind regards,
Dries.

0 Kudos