NHS3152 ADCSP Setting Description

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

NHS3152 ADCSP Setting Description

1,491 次查看
bmeyer
Contributor II
破坏者
On the NHS3152 ADCSP (ADC set up) register, bit 0 is labeled as "ADOFFSETCAL" but description has a measurement refence voltage. Can you explain?

Plus should correspond to ADC input range setting. Can you explain how these two settings are to be aligned and why?
2 回复数

1,486 次查看
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Please find more information as the document.

URL:https://www.nxp.com/docs/en/user-guide/UM10876.pdf.

Hope it help you. Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 项奖励
回复

1,170 次查看
jesmith
Contributor III

There isn't more information in the document @fangfang points us to. Can anyone at NXP comment more definitively? 

0 项奖励
回复