NHS3100UCODEADK information and SDK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NHS3100UCODEADK information and SDK

1,115件の閲覧回数
Kralg
Contributor I

Hello,

I am trying to understand more about NHS3100UCODEADK.Can you please write where to find the SDK?

It is also written that there are two ICs and Rain RFID, but the main chip is HF, can you please extend the description so what frequencies does it support? UHF and HF?

In general the information is very scarce, does it mean this Board or SL354011FHK  is discontinued? Do you have some boards for UHF with sensors ?

0 件の賞賛
返信
2 返答(返信)

1,091件の閲覧回数
patrickgeens
NXP Apps Support
NXP Apps Support

Hi Kraig,

 

1) Due to a change in licensing SDK 12.5 is being replaced with SDK 12.6, which will be released for download end of this week. Our apologies for the temporary unavailability.

2) The main components on the NHS3100UCODE board are:

- NHS3100 with a NFC interface at 13.56MHz (magnetic coupling, typical distances up to 4cm, depending on antenna and reader)
- SL3S4011 with UHF interface in the 860 to 960 MHz band (typical distances in meters range depending on antenna and reader)

3) The SL3S4011 does not support energy harvesting for external sensors. I am not aware of  demo boards supporting UHF powered sensors.

 

Kind regards,

Patrick

 

 

 

1,054件の閲覧回数
patrickgeens
NXP Apps Support
NXP Apps Support

Hi Kraig,

 

Version 12.6 of the SDK is now available on the website:

https://www.nxp.com/products/rfid-nfc/nfc-hf/ntag-smartsensor/ntag-smartsensor-with-temperature-sens...

 

Kind regards,

Patrick

 

 

0 件の賞賛
返信