NHS3100 Adherance monitoring has not yet started

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NHS3100 Adherance monitoring has not yet started

1,199件の閲覧回数
rnd1
Contributor I

Hi,

I'm using NHS3100 therapy adherence. flash firmware www.nxp.com/downloads/en/apps/
app_demo_dp_tadherence_gpio14.bin file into NHS3100 using mobile app NHS31xx Downloader.

By using the NXP Therapy Config app started therapy successfully.

When i sacn NFC it shows "Adherance monitoring has not yet started"

I don't understand the issue. Please help to solve this issue.

0 件の賞賛
返信
2 返答(返信)

1,118件の閲覧回数
driesmoors
NXP Employee
NXP Employee

Hi,

  • Can you retry using the binary in the latest SDK?
  • Can you check if the switches are all down (== "not extracted from the cavity")?
  • Are you sure the IC is reset after a firmware flash? The best way to do is - which also guarantees to clear all HW debug breakpoints - is to physically remove the battery and re-insert it after flashing.

Kind regards,
Dries.

0 件の賞賛
返信

1,118件の閲覧回数
fangfang
NXP TechSupport
NXP TechSupport

Hello,

 I can't reproduce your issue for it and please find the test as the attached. You may check your board battery.

Have a nice day.

0 件の賞賛
返信