NFC pn548(npc300) is not working with linux_libnfc-nci after rerun nfcDemoapp

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NFC pn548(npc300) is not working with linux_libnfc-nci after rerun nfcDemoapp

3,972 Views
JarvisC
Contributor II

Dear NXP,

 

After download linux_libnfc-nci from "https://github.com/NXPNFCLinux/linux_libnfc-nci.git", and modified I2C_BUS / I2C_ADDRESS / PIN_INT and PIN_ENABLE in linux OS Cent OS /Ubuntu OS, the NFC could work normal with nfcDemoapp , but it could not be re-run with nfcDemoapp tool with error message "Too many i2c read errors: ABORTING".

 

Please help to share the related information that could help me to debug/fix this defect?

 

Thanks.

0 Kudos
Reply
3 Replies

2,593 Views
fury-1984
Contributor I

Hello
How did you set the desired pins?(I2C_BUS / I2C_ADDRESS / PIN_INT and PIN_ENABLE )

0 Kudos
Reply

3,965 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello @JarvisC .

Unfortunately, we don't have rights to support this product PN548. It is a NFC chip using in Mobile application. Specially supported by a mobile team in NXP. Please contact the local distributor or NXP marketing to request for special support.

Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 Kudos
Reply

3,951 Views
JarvisC
Contributor II

Dear NXP,

After debug the problem , I found that's related the error "_i2c_read() errno :79 ".

The error message is also reproduced on Cent7  and Ubuntu 18.04.6 OS.

Does anyone have any idea that could help to fix the defect?

Thanks.

0 Kudos
Reply