NFC pn544 firmware update failed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NFC pn544 firmware update failed

2,009件の閲覧回数
yenchou
Contributor III

Hello All,

I used Android6.0.

NFC modules  firmware version is 8.1.13.

NFC  firmware file version is  8.1.26.

I have a problem is "NxpHal : FW Download failed - NFCC init will continue".

This is the log:


04-18 08:23:23.198 868 1064 D NxpExtns: const nxp::CNfcParam* nxp::CNfcConfig::find(const char*) const found NXPLOG_FWDNLD_LOGLEVEL=(0x3)
04-18 08:23:23.198 868 1064 D : phNxpLog_InitializeLogLevel: global =1, Fwdnld =3, extns =3, hal =3, tml =3, ncir =3, ncix =3
04-18 08:23:23.508 868 1073 D NxpHal : NxpNci> FW Version: 8.1.13
04-18 08:23:23.508 868 1064 D NxpFwDnld: Allocating Mem for Dnld Context..
04-18 08:23:23.508 868 1064 D NxpExtns: const nxp::CNfcParam* nxp::CNfcConfig::find(const char*) const found NXP_FW_NAME=libpn547_fw.so
04-18 08:23:23.536 868 1064 D NxpFwDnld: @@@/system/vendor/firmware/libpn547_fw.so
04-18 08:23:23.536 868 1064 D NxpFwDnld: FW Image Length - ImageInfoLen 34590
04-18 08:23:23.536 868 1064 D NxpFwDnld: FW Image Info Pointer - pImageInfo af5712d0
04-18 08:23:23.536 868 1064 D NxpFwDnld: FW Major Version Num - 1
04-18 08:23:23.536 868 1064 D NxpFwDnld: FW Minor Version Num - 26
04-18 08:23:23.536 868 1064 D NxpFwDnld: FW Image Length - 34590
04-18 08:23:23.536 868 1064 D NxpFwDnld: FW Image Info Pointer - af5712d0
04-18 08:23:23.536 868 1064 D NxpHal : FW version for FW file = 0x126
04-18 08:23:23.536 868 1064 D NxpHal : FW version from device = 0x80113
04-18 08:23:23.536 868 1064 D NxpHal : phNxpNciHal_CheckValidFwVersion current_major_no = 0x1
04-18 08:23:23.536 868 1064 D NxpHal : FW update required
04-18 08:23:23.537 868 1064 D NxpFwDnld: gphNxpNciHal_fw_IoctlCtx.bClkSrcVal = 0x1
04-18 08:23:23.537 868 1064 D NxpFwDnld: gphNxpNciHal_fw_IoctlCtx.bClkFreqVal = 0x0
04-18 08:23:23.537 868 1064 D NxpFwDnld: gphNxpNciHal_fw_IoctlCtx.bClkFreqVal = 0x1
04-18 08:23:23.537 868 1064 E NxpFwDnld: Clock frequency value is wrong in config file, setting it as default
04-18 08:23:23.775 868 1064 D NxpHal : Calling Seq handler for FW Download
04-18 08:23:23.775 868 1064 D NxpExtns: const nxp::CNfcParam* nxp::CNfcConfig::find(const char*) const found NXP_FW_NAME=libpn547_fw.so
04-18 08:23:23.777 868 1064 D NxpFwDnld: @@@/system/vendor/firmware/libpn547_fw.so
04-18 08:23:23.777 868 1064 D NxpFwDnld: FW Image Length - ImageInfoLen 34590
04-18 08:23:23.777 868 1064 D NxpFwDnld: FW Image Info Pointer - pImageInfo af5712d0
04-18 08:23:23.777 868 1064 D NxpFwDnld: FW Major Version Num - 1
04-18 08:23:23.777 868 1064 D NxpFwDnld: FW Minor Version Num - 26
04-18 08:23:23.777 868 1064 D NxpFwDnld: FW Image Length - 34590
04-18 08:23:23.777 868 1064 D NxpFwDnld: FW Image Info Pointer - af5712d0
04-18 08:23:23.777 868 1064 D NxpFwDnld: phDnldNfc_InitImgInfo:SUCCESS
04-18 08:23:23.777 868 1064 D NxpFwDnld: Processing R/W Sequence..
04-18 08:23:23.777 868 1064 D NxpFwDnld: Response Timer Created Successfully
04-18 08:23:23.777 868 1064 D NxpFwDnld: Inserting FrameId ..
04-18 08:23:23.777 868 1064 D NxpFwDnld: Frame created successfully
04-18 08:23:23.777 868 1064 D NxpFwDnld: Force Command Request submitted successfully
04-18 08:23:23.792 868 1073 D NxpFwDnld: Send Success
04-18 08:23:23.792 868 1073 D NxpFwDnld: Response timer started
04-18 08:23:23.792 868 1073 E NxpFwDnld: Invalid frame received
04-18 08:23:23.792 868 1073 E NxpFwDnld: phNxpNciHal_fw_dnld_normal_cb - Request Failed!!
04-18 08:23:23.792 868 1064 D NxpFwDnld: Processing R/W Sequence..
04-18 08:23:23.792 868 1064 D NxpFwDnld: Response Timer Created Successfully
04-18 08:23:23.792 868 1064 D NxpFwDnld: Inserting FrameId ..
04-18 08:23:23.792 868 1064 D NxpFwDnld: Frame created successfully
04-18 08:23:23.792 868 1064 D NxpFwDnld: Force Command Request submitted successfully
04-18 08:23:23.802 868 1073 D NxpFwDnld: Send Success
04-18 08:23:23.802 868 1073 D NxpFwDnld: Response timer started
04-18 08:23:23.824 868 1073 E NxpFwDnld: Invalid frame received
04-18 08:23:23.824 868 1073 E NxpFwDnld: phNxpNciHal_fw_dnld_normal_cb - Request Failed!!
04-18 08:23:23.825 868 1064 D NxpFwDnld: Processing Normal Sequence..
04-18 08:23:23.825 868 1064 D NxpFwDnld: Initializing Sequence..
04-18 08:23:23.825 868 1064 D NxpFwDnld: Response Timer Created Successfully
04-18 08:23:23.825 868 1064 D NxpFwDnld: Inserting FrameId ..
04-18 08:23:23.825 868 1064 D NxpFwDnld: Frame created successfully
04-18 08:23:23.825 868 1064 D NxpFwDnld: GetSessionState Request submitted successfully
04-18 08:23:23.836 868 1073 D NxpFwDnld: Send Success
04-18 08:23:23.836 868 1073 D NxpFwDnld: Response timer started
04-18 08:23:23.844 868 1073 E NxpFwDnld: Invalid frame received
04-18 08:23:23.844 868 1073 E NxpFwDnld: phNxpNciHal_fw_dnld_get_sessn_state_cb - Request Failed!!
04-18 08:23:23.845 868 1064 E NxpFwDnld: phDnldNfc_GetSessionState cb failed
04-18 08:23:23.845 868 1064 E NxpFwDnld: phNxpNciHal_fw_seq_handler : FAILED
04-18 08:23:23.845 868 1064 D NxpFwDnld: phNxpNciHal_fw_dnld_complete: Download Status = 0xff
04-18 08:23:23.845 868 1064 E NxpFwDnld: Fw Download Failed!!
04-18 08:23:23.957 868 1064 E NxpFwDnld: free library SUCCESS !!
04-18 08:23:23.957 868 1064 E NxpFwDnld: Freeing Mem for Dnld Context..
04-18 08:23:23.957 868 1064 E NxpHal : FW Download failed - NFCC init will continue
04-18 08:23:29.046 868 1060 D NxpExtns: const nxp::CNfcParam* nxp::CNfcConfig::find(const char*) const found NXPLOG_FWDNLD_LOGLEVEL=(0x3)
04-18 08:23:29.046 868 1060 D : phNxpLog_InitializeLogLevel: global =1, Fwdnld =3, extns =3, hal =3, tml =3, ncir =3, ncix =3

So I could not download the FW file to update the nfc module.

Could anyone help me to solve the problem? 

 

Thank you with your help.

Have a great day,

Yen

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,470件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Yen,

PN544 is for mobile application , and it is supported by a dedicated team, but not included in the mass market range, please kindly contact your local DFAE for support on this, and they have the channel to that team.

Please kindly refer to Distributor Network|NXP  for more details.


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------