NFC - passive card removal detection

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NFC - passive card removal detection

ソリューションへジャンプ
1,274件の閲覧回数
me3
Contributor I

in regard to the PN7120:
is there a way to passively detect when a NFC device/card is physically removed from the chip?
android, in recent versions, supports this, and i would like replicate this behaviour with my NXP NFC hardware.

0 件の賞賛
1 解決策
1,115件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Alex,

Thanks for the clarification! Referring to UM10819, it can not detect the card removal without MCU side's activity, please refer to the following for more details.

pastedImage_1.png

Have a great day,
Kan

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

5 返答(返信)
1,115件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Yes, such kind of event can be detected. Please refer to the following for more details.

pastedImage_2.png

Have a great day,
Kan

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
1,115件の閲覧回数
me3
Contributor I

thank your for your reply, but i am not sure what you are suggesting?
i am specifically looking for a way to passively detect card removal.
WITHOUT sending commands to the nfc card, as i must not disrupt the communication flow.
this is in regard to nfc chipcards not simple tags.

0 件の賞賛
1,115件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

What do you mean "WITHOUT sending commands to the nfc card"? Would you please specify the use case? Generally when the card is close to the device, the communication would start automatically. Do you want the PN7120 report this kind of event when the card is suddenly removed during the communication? Please kindly clarify.

Have a great day,
Kan

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
1,115件の閲覧回数
me3
Contributor I

we built a NFC card reader based on PN7120. we connect it to a smartphone or PC and use it to read e.g. credit cards or government IDs. the command APDUs come from the connected device, the reader just passes them through. the reader is not allowed to send its own APDUs to the card, as this would potentially interrupt the communication between the card and the device.

now we want to detect when a connected card is removed from the reader. we need to do so without sending any APDUs (detect passively, not actively).

android has a feature to achieve exactly that, with the built in NFC hardware already.

we want to know if this is possible with the PN7120 in our reader as well and if so, how?

thanks for your help!

0 件の賞賛
1,116件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Alex,

Thanks for the clarification! Referring to UM10819, it can not detect the card removal without MCU side's activity, please refer to the following for more details.

pastedImage_1.png

Have a great day,
Kan

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------