NFC field couldn't wake up the NHS3100

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NFC field couldn't wake up the NHS3100

777 Views
shadyelmakhzang
Contributor I

Hi Everybody,

I have an NHS3100 Board with some FW and without any battery supplies.

When I tried to power it up with an NFC field while the Reset pin is floating, it wakes up and works properly.

However, When I connect the Reset pin to a scope or to a GPIO from another Powered-off controller, the NFC field couldn't power up the board and it doesn't work properly.

Do you have an explanation of the difference between the two scenarios?

Thanks,

Shady R. Elmakhzangy

Labels (1)
Tags (3)
0 Kudos
3 Replies

575 Views
driesmoors
NXP Employee
NXP Employee

Hi,

The only explanation I can come up with is that somehow the RESETN pin is pulled low, bringing the IC in reset. Can you check the impedance of the scope or the other controller?

Best,
Dries.

575 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Is the board NHS3100 Starter Kit for Temperature Monitoring|NXP ? Please kindly clarify.


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

575 Views
shadyelmakhzang
Contributor I

Yes it is!

0 Kudos