NFC PN7150 porting on Android Oreo 8.1 - nxpnfc_hal_svc crash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NFC PN7150 porting on Android Oreo 8.1 - nxpnfc_hal_svc crash

4,212 Views
hannywei
Contributor I

Dear

Transplant PN7150 to I.MX8Mq with reference AN11690.pdf, which runs android O 8.1.0_1.3.0
we have followed steps of AN11690, even found some issue like https://community.nxp.com/thread/489133, while modified following the link, but also can not work.

logcat:(the attachment is the details)
12-20 01:05:15.830 3693 3693 E android.hardware.nfc@1.0-impl: hw_get_module nfc_nci failed: -2
12-20 01:05:15.830 3693 3693 E android.hardware.nfc@1.0-impl: Passthrough failed to load legacy HAL.
12-20 01:05:15.830 3693 3693 E vendor.nxp.nxpnfc@1.0-service: Could not get passthrough implementation for android.hardware.nfc@1.0::INfc/default.
12-20 01:05:15.830 3693 3693 F vendor.nxp.nxpnfc@1.0-service: Error while registering nfc AOSP service: 1
12-20 01:05:15.830 3693 3693 F libc : Fatal signal 6 (SIGABRT), code -6 in tid 3693 (vendor.nxp.nxpn), pid 3693 (vendor.nxp.nxpn)
12-20 01:05:15.831 2782 2782 E ActivityRecognitionHardware: activity_recognition HAL is deprecated. class_init is effectively a no-op
12-20 01:05:15.853 3713 3713 I crash_dump64: obtaining output fd from tombstoned, type: kDebuggerdTombstone
12-20 01:05:15.854 3358 3358 I /system/bin/tombstoned: received crash request for pid 3693
12-20 01:05:15.854 2782 2782 W Zygote : Class not found for preloading: android.icu.impl.number.Parse
12-20 01:05:15.856 3713 3713 I crash_dump64: performing dump of process 3693 (target tid = 3693)
12-20 01:05:15.856 3713 3713 F DEBUG : *** *** *** *** *** *** *** *** *** *** *** *** *** *** *** ***
12-20 01:05:15.856 3713 3713 F DEBUG : Build fingerprint: 'Android/paicheng_8mq/paicheng_8mq:8.1.0/1.3.0-rfp-rc3/20180406:userdebug/dev-keys'
12-20 01:05:15.856 3713 3713 F DEBUG : Revision: '0'
12-20 01:05:15.856 3713 3713 F DEBUG : ABI: 'arm64'
12-20 01:05:15.856 3713 3713 F DEBUG : pid: 3693, tid: 3693, name: vendor.nxp.nxpn >>> /system/bin/hw/vendor.nxp.nxpnfc@1.0-service <<<
12-20 01:05:15.856 3713 3713 F DEBUG : signal 6 (SIGABRT), code -6 (SI_TKILL), fault addr --------
12-20 01:05:15.858 3713 3713 F DEBUG : Abort message: 'Error while registering nfc AOSP service: 1'
12-20 01:05:15.858 3713 3713 F DEBUG : x0 0000000000000000 x1 0000000000000e6d x2 0000000000000006 x3 0000000000000008

Questions:
1. why can not find INfc/default?
2. Is that right about the following changes of step 7,otherwise,how to do?

All the changes:
1. download kernel driver followed installation instructions.
2. download patch and run "./NxpNfcAndroid/install_NFC.sh", all successfully.
3. device/fsl/imx8/paicheng_8mq.mk:
# add nfc hal
PRODUCT_PACKAGES += \
NfcNci \
Tag \
com.nxp.nfc \
android.hardware.nfc@1.0-impl \
vendor.nxp.nxpnfc@1.0-impl \
vendor.nxp.nxpnfc@1.0-service \
nfc_nci.pn54x


PRODUCT_COPY_FILES += \
frameworks/native/data/etc/android.hardware.nfc.xml:system/etc/permissions/android.hardware.nfc.xml \
frameworks/native/data/etc/android.hardware.nfc.hce.xml:system/etc/permissions/android.hardware.nfc.hce.xml \
frameworks/native/data/etc/android.hardware.nfc.hcef.xml:system/etc/permissions/android.hardware.nfc.hcef.xml \
NxpNfcAndroid/conf/libnfc-brcm.conf:$(TARGET_COPY_OUT_VENDOR)/etc/libnfc-brcm.conf \
NxpNfcAndroid/conf/libnfc-nxp.conf:$(TARGET_COPY_OUT_VENDOR)/etc/libnfc-nxp.conf \
NxpNfcAndroid/conf/libnfc-nxp_RF.conf:$(TARGET_COPY_OUT_VENDOR)/libnfc-nxp_RF.conf

4. device/fsl/paicheng_8mq/manifest.xml
<hal format="hidl">
<name>android.hardware.nfc</name>
<transport>hwbinder</transport>
<impl level="generic"></impl>
<version>1.0</version>
<interface>
<name>INfc</name>
<instance>default</instance>
</interface>
</hal>
<hal format="hidl">
<name>vendor.nxp.nxpnfc</name>
<transport>hwbinder</transport>
<impl level="generic"></impl>
<version>1.0</version>
<interface>
<name>INxpNfc</name>
<instance>default</instance>
</interface>
</hal>
5. vi system/core/rootdir/init.rc

on post-fs-data
...
# add for NFC
#mkdir /data/vendor 0777 nfc nfc #should comment this , before have mkdir /data/vendor 0771 root root
mkdir /data/vendor/nfc 0777 nfc nfc
mkdir /data/vendor/nfc/param 0777 nfc nfc
setprop ro.nfc.port "I2C"
chmod 0660 /dev/pn544
chown nfc nfc /dev/pn544

6. system/sepolicy/tests/treble_sepolicy_tests.py
added hal_nfc_default to coredomainWhilelist to solve build error.

coredomainWhitelist = {
'adbd',
'kernel',
'postinstall',
'postinstall_dexopt',
'recovery',
'system_server',
'modprobe',
'hal_nfc_default',
}

7. system/libhidl/transport/ServiceManagement.cpp
for (const std::string &lib : libs) {
const std::string fullPath = path + lib;

#if 0
if (path != HAL_LIBRARY_PATH_SYSTEM) {
handle = android_load_sphal_library(fullPath.c_str(), dlMode);
} else {
handle = dlopen(fullPath.c_str(), dlMode);
}
#else
handle = dlopen(fullPath.c_str(), dlMode);
#endif

0 Kudos
Reply
3 Replies

3,093 Views
zli
Contributor I

I have the same problem, how to solve it?

0 Kudos
Reply

3,093 Views
larkin_lai
Contributor I

Hi Hanny 

 I faceed the same problem.have you solved this problem?

0 Kudos
Reply

3,093 Views
vizhen_tan
Contributor I

You can  try added this in you device.mk:

    PRODUCT_PACKAGES += \

      com.nxp.nfc \

      com.nxp.nfc.xml

0 Kudos
Reply